5/18/07 Fixed bug that caused an exception to be thrown when right clicking on
   a chart with no data channels 'enabled.
Added missing Tracking Cursor combobox menuitem to the "View|Chart|Tracking Cursor" menu.
Added "Apply Changes" menu item to the Tracking Cursor menus, and reworked their functionality.

09/08/08 to 10/31/08 Version 1.04 Release Notes.
- New Features................................................................
- Added more channels so that the total is now 48.  Customer request.
- Added choices for 1000, 2000, 4000, 8000, 16000, or 32000 data points.  Customer request.
- Modified charting and data logging so that Ambient can be charted/logged along with process.
   This is needed for the UWRH units, where customers want to plot temperature with RH.
- Added Offset Calibration to Channel Configuration.
- Added support for configuring MWTC and UWRH connectors.
- Added support for configuring MWTC-REC1 receivers.
- Added Japanese color codes to View menu for Channels display.
- Modified Configuration Wizards so that only USB serial ports are checked when connecting.
- Optimized connection code in Wizards so that establishing a link to a device happens more
   rapidly.
- Modified Wizards to show Device Model Number, Firmware version, and Wizard software version.
- Modified TC Central to search only USB serial ports, reducing connect time at startup.
- Added code to detect insertion and removal of USB devices, so that the main program will
   report "No Connection" when the receiver USB plug is removed, and automatically re-
   connect when the same plug is re-inserted.
- Updated splash screen and about box to read "Omega Wireless Products" instead of UWTC.

- Bug Fixes...................................................................
- Fixed bug that would not allow a saved data file to be loaded.
- Fixed bug that randomly caused the program to "freeze" or lock up on exit.
- Fixed bug that caused TC Central to use 50% PC resources.

04/27/09 Release Notes for Version 1.04.9.427 maintenance release
- Bug Fixes...................................................................
- Fixed bug that caused chart time labels to be incorrect when charting in
   "Continuous" mode, and the maximum number of data points have been plotted.
- Fixed bug that caused incorrect update of alarm settings when selecting
   units in Deg C.  (This was reported by a customer)
- Removed the radio buttons on the channel configuration dialog box and 
   replaced with a label that shows the currently selected "Temperature" 
   units.  Relative humidity and future products with pressure mV, etc. are 
   not affected by this change.  Temperature units are now selected from the
   main "Channels" tabs only.  This reduces confusion and prevents displaying
   readings in one temperature unit while having to choose between units
   when configuring alarm and/or offsets.
- Fixed bug that caused incorrect readings when an offset value is specified,
   and readings are being viewed in Deg C.

05/12/09 Release Notes for Version 1.04.9.512 maintenance release
- Bug Fixes...................................................................
- Expanded the UpDown Control for Emissivity in the End Device Configuration
   Wizard, to allow for user Windows System settings with "Large Fonts".

06/11/09 Release Notes for Version 1.05.9.611 new version release

- New Features................................................................
- Added support for Wireless IR Gun, which displays process temperature but
   not Ambient.  Also displays "OMEGASCOPE" in the empty space below the
   process temperature window, to give the box a less "vacant" appearance.

- Added "Save Channel Configuration" and "Open Channel Configuration" so that
   an existing installation and setup of multiple channels can be saved, and
   reloaded when upgrading to a new version of TCC.  This also allows the user
   to create and save multiple configurations for different applications.

- Added support for MWTC-REC5 in the End Device Configuration Wizard.

- Added Activate Master Remote Alarm for REC2/4/6.  This allows the user to
   select which channel(s) will activate the alarm output on receivers with
   analog output.  This feature only works when the receiver is plugged into
   a USB port, and TCC is running.  If the USB cable is unplugged, only the
   channel assigned to the receiver's analog output will operate.  To that
   extent, if the alarm output is activated because of a channel other than
   the assigned analog channel, the alarm will clear upon removal of the
   USB cable.

- Bug Fixes...................................................................
- Fixed bug in the "Line Options" dialog box listbox where the selected line
   was not the same line as the one selected in the listbox.

08/21/09 Release Notes for Version 1.05.9.821 maintenance release
- Bug Fixes...................................................................
- Fixed bug that caused all zeros for addresses in channel boxes, and a 
   crash when configuring a channel.  The default.bsf file was from an older
   version, which caused channel data to become corrupted.

08/31/09 Release Notes for Version 1.05.9.831 maintenance release
- Bug Fixes...................................................................
- Disabled temperature conversion that takes place when clicking on the C or F
   button (for TCType O only), but allow display units to change.  Also
   disabled temperature conversion in data log for TCType "O".  Note:  Charting
   changes the vertical axis when the C/F button is pressed, so the value for
   IR Guns stays as transmitted C/F, regardless of the C/F button setting.  In
   other words, the C/F button settings must match the C/F settings on the IR
   Gun.  When data logging, all channels must be set to the same units as the
   IR Gun, even if monitoring thermocouples concurently.

09/01/09 Release Notes for Version 1.05.9.901 maintenance release
- Bug Fixes...................................................................
- Added special configuration dialog box for Type O transmitters, so that the
   user can notify TC Central whether the IR Gun is transmitting in Deg C or
   Deg F.  This fixes all the known problems reported since version 1.5.9.611.
   Changes made for version 1.5.9.831 have been un-done, since they caused
   problems with charting and data logging.  This release reports temperatures
   correctly (if the user sets it up properly), and has no side effects with
   charting or data logging.

10/14/09 Release Notes for Version 1.06.9.1014 new version release

- New Features................................................................
- Added support for UWPC - Universal Wireless Process Transmitter.  Features
   include choice of signal source (V0, V1, V2, MA), process units, custom
   units, and scalling for the channel display and chart/log.  Scaling can
   also be used for field calibration by the customer.

- Added support the UWTC-REC2 Rev B - 2.4GHz Receiver with analog output.  
   This includes scaling of the analog output, choice of process units, 
   ambient units, alarm setpoint, activation mode, deadband, and master 
   alarm  activation.  Scaling can also be used for field calibration by the 
   customer.

- Added support for UWTC-REC4 - 2.4GHz Receiver with 4 analog outputs.  This
   includes scaling of each individual analog output, choice of process units,
   alarm setpoint, activation mode, deadband, and master alarm activation.
   Scaling can also be used for field calibration by the customer.

- Added support for MWTC-REC6 - 868/915MHz Receiver with Analog Output. This
   includes scaling of the analog output, choice of process units,
   and RF channel selection.  Scaling can also be used for field calibration
   by the customer.

- Combined receiver configuration with TC Central, so that the receiver
   can be configured while TC Central is running.  It is now a menu option,
   and the UWTC Receiver Configuration Wizard no longer exists.

- Re-coded receiver connection for faster, more reliable connection.

- Added the "Find Devices" menu option in the "Tools" menu, which
   allows the user to view all transmitters being received, along with
   their address.  This is useful if you don't remember or know the
   address of a particular end device.

11/25/09 Release Notes for Version 1.06.9.1125 maintenance release
- Bug Fixes...................................................................
- Fixed bug in end device configuration wizard that prevented settings for
   UWTC-2-NEMA and UWRTD-2-NEMA TC type and RTD type from being sent to
   the end device.

12/21/09 Release Notes for Version 1.07.9.1221 new version release

- New Features................................................................
- Modified reciever configuration code to allow user to change RF Network
   settings for RF Channel, PAN ID, and Receiver (Destination) Address.  This
   change is for UWTC-REC1/REC2/REC2D/REC4, UWRPT-915/868, and all UWTC 2.4GHz
   end devices.  The MWTC receivers and end devices remain unchanges.  This
   change was required to allow the use of multiple UWRPT repeaters, as
   requested by a potential customer.

- Added an additional 4 Channel tabs to accomodate a total of 96 end devices.
   This changes was required to allow the use of multiple UWRPT repeaters,
   with two sets of 40 end devices as requested by a potential customer.

- Added support for UWRPT-915/868 - Universal Wireless Repeater.  The UWRPT
   can be configured as an end device with the End Device Configuration
   Wizard or with "Configure Receiver" from the "Tools" menu in TCC.  With the 
   USB cable attached and TCC running, the UWRPT can be used as a mid-point 
   2.4GHz receiver to monitor end devices, while simultaneously 
   re-transmitting at 915/868MHz.

- Modified receiver configuration code to allow user to adjust an offset
   for TC-K analog output for the UWTC-REC2(D)-TC/REC4-TC.  This change was
   in response to multiple customer requests.

- Added support for UWTC-REC2/REC2D-NEMA.  The UWTC-REC1-NEMA is not supported
   because the hardware and firmware are unknown at the time of this release.
   This will be treated as a bug fix in the next maintenance release, if the
   next new version release is delayed.

- Added support for UWXL-24-TC and UWXL-24-RTD.

- Bug Fixes...................................................................
- Fixed bug that caused an exception to be thrown when upgrading TC Central
   from versions older than 1.6.

- Removed "Thousands Separator" (comma), from the scaling numeric up-down
   controls in the UWTC-REC2/REC4 receiver configuration dialog boxes.

- Renamed the title bar of the UWTC-REC4 dialog box from "dlgRec4" to
   "Configure Receiver".

- Fixed bug that caused "Thermocouple Type K Output is Not Scalable"
   to remain visible when unplugging a UWTC-REC2/REC4-TC receiver while
   TCC is still running and plugging in a UWTC-REC2/REC4-V1/V2/MA, and then
   choosing "Configure Receiver" again.  This bug does not appear if TCC is
   shut down and restarted with the second receiver.  It is highly unlikely 
   that a customer would find themselves in this situation, but it is an
   annoyance (and added labor expense) for factory production personnel to 
   have to restart TCC when configuring and testing receivers.

- Modified placement of various panels in the "Scaling" group box of the
   UWTC-REC2/REC4 configuration dialog boxes in an attempt to fix a 
   non-reproducalbe bug that caused some of the labels and controls to be 
   partially hidden.  This bug was reported by only one user running
   Windows XP, and could not be re-produced at Omega South.

12/22/09 Release Notes for Version 1.07.9.1222 maintenance release

- Bug Fixes...................................................................
- Fixed bug that caused incorrect readings with the UWPC-2-NEMA/USCA when
   configured for V1 (0-5V).

01/07/10 Release Notes for Version 1.08.10.0107 new version release

- New Features................................................................
- Added support for the MWTC-x-868S, for use in Singapore.

- Bug Fixes...................................................................
- Fixed bug that caused MWTC connectors to not be recognized by the
   End Device Configuration Wizard.  This bug was introduced when changes
   for the UWRPT were made(Version 1.07.9.1221).

01/20/10 Release Notes for Version 1.08.10.0120 maintenance release

- Bug Fixes...................................................................
- Fixed bug that caused the End Device Configuration Wizard to throw an
   exception when configuring a UWRTD-2-NEMA end device.

02/09/10 Release Notes for Version 1.08.10.0209 maintenance release

- Bug Fixes...................................................................
- Fixed bug that caused Nevron watermark to appear on the chart window, by
   re-installing license key.


04/09/10 Release Notes for Version 1.09.10.0409 new version release

- New Features................................................................

- Added support for the UWPH, which includes field probe calibration.

- Added support for the UWTC-REC6.

- Removed 4 tabs from Channels view to reduce the number of channels from
   96 to 48.  CCF file size is still the same and array size is still 96.
   Only the first 48 elements of the arrays are used.

- Added support for correct battery status when using a 1.5V/1.8V battery.
   If battery voltage is below 1.90V, it is assumed that a 1.5/1.8 battery is
   in use, and 1.25V to 1.5V is scaled to 0 to 100%.  If battery voltage is
   1.90V or above, 2.50V to 3.3V is scaled to 0 to 100%.

- Bug Fixes...................................................................
- Fixed bug that caused REC2/REC4 to fail response to TCOS command when the
   users PC has a regional setting for a culture that doesn't support the use
   of a period for a decimal poiont.

- Fixed bug that caused the alarm setpoints and offset calibration in the
   configure channel dialog box to remain in degrees F, even when the "C"
   button is selected in the channel box.

- Fixed bug that caused offset values in the configure channel dialog box
   to not have the same number of decimal places as displayed in the channel
   box for process value.

- Removed "Transmission in C" checkbox from receiver configuration dialog
   box for all UWTC-RECx receivers.

- Fixed bug that caused the data log to log the value of the device in
   the column to the left to be recorded instead of 0, if the device is
   either lost or powered off during a logging session.

- Fixed bug that caused the MWTC-REC6 to not change channels after 
   configuration.

05/13/10 Release Notes for Version 1.09.10.0513 maintenance release

- Bug Fixes...................................................................
- Fixed bug that caused the Channel Timeout to be set to 60 when the user
   attempts to set it to any value above 120.  This was bug was present since
   the original version 1.0 release of 05/18/07 where values up to 120 were
   allowed (by program design), but reset to 60 if the value exceeded 120.  
   The new limits are now 6 seconds minimum and 3600 seconds maximum.

06/14/10 Release Notes for Version 1.09.10.0614 maintenance release

- Bug Fixes...................................................................
-  Fixed bug in the end device configuration wizard that caused the error
   message "End device failed to respond to TCTYPE" for UWRTD-2-NEMA units
   with firmware 091216 and older only.  The bug was related to a change made
   in Version 1.08.10.0120, where older firmware reported "UWTRD2NEMA" and TCC
   expected "UWRTD2NEMA".  That and newer releases of TCC did not recognize
   "UWTRD2NEMA" as a valid end device, so hence the error message.  Now both 
   unit ID's are recognized as UWRTD-2-NEMA.

-  Changed error message for unrecognized end devices to a more meaningful,
   "Unrecognized End Device.  Please check omega.com for a newer version of TC
   Central."

07/13/10 Release Notes for Version 1.10.10.0713 new version release
- New Features................................................................

- Added support for the UWXL-24-PH, UWXL-24-IR-1, UWXL-24-RH-RPI, and 
   UWXL-24-PC.  The UWXL-24-FQ will be added later when the UWFL is completed.

08/04/10 Release Notes for Version 1.10.10.0804 maintenance release

- Bug Fixes...................................................................
-  This release adds support for the UWTC-RPT-868, but is treated as a bug
   fix in a maintenance release rather than a new feature in a new version 
   release, since the revision history of 12/21/09 alludes to support being 
   added for the "UWRPT-915/868".  One notable difference in the Configuration 
   Wizard for the 868 model is "RF Channel" is grayed out and set to 1, and
   "Receiver Address" is grayed out and set to 0.  This is because the 868MHz
   modules do not support more than one channel, and only the destination
   address can be changed.

09/01/10 Release Notes for Version 1.10.10.0901 maintenance release

- Bug Fixes...................................................................
- Fixed bug that caused an exception to be thrown when starting a data logging
  session.  This exception only occured when one or more channel boxes have
  an empty description fields.



11/08/10 Release Notes for Version 1.10.10.1108 maintenance release

- Bug Fixes...................................................................
- Although not included in release notes for version 1.10.10.901, a bug in the
  checksum function was fixed that caused the function to always return the
  correct checksum, even if the received packet was corrupted.  This fix 
  caused all MWTC packets to be reported as being corrupt and having a bad 
  checksum.  The cause was determined to be a two-year old bug in the MWTC 
  receiver firmware, which included the packet length in the checksum 
  calculation, which should not be done.  The firmware bug cannot be fixed 
  because of its age and the number of units sold.  In order to ensure a valid
  checksum, this release of TCC takes into account the receiver type in the
  checksum function, and adds the packet length to the checksum calculation on
  packets received from MWTC receivers.




12/13/10 Release Notes for Version 1.11.10.1213 new version release

- New Features
-  Added support for DPG409 pressure sensor and HHF1000 air velocity sensor.
-  Added data logging auto-save feature.  As a result, user now needs to pick
a filename at the start of data logging.
-  Reorganized .csv output file to support auto-save.  There is now a single data
section, at the bottom of the file.
-  Added Configure Axes button. Allows renaming of left and right axes on chart.
-  Process and Ambient from each device can be independently placed on left or
right axis.
-  Added Options button to each channel box for configuring units, offsets, etc.
(Can still be accessed with Right Click-->Configure as before).
-  Display Units and Logging Units can be set separately for each device. 
Display Units are what appear in the main channel box, and can be set by clicking
the Options button on that channel box. This can be changed at any time. 
Logging Units are selected when data logging begins, and can not be changed during 
data logging.
-  Removed "F" and "C" buttons in favor of new Display Units and Logging Units
settings.  There are now so many non-temperature devices that these no longer made 
sense.  This also simplifies program's internal data storage and output file.


- Bug Fixes
-  Fixed End Device Configuration Wizard bug where Step # always increased.
-  Updated transmission frequency display for UWTC-RPT-868 to 869.525 MHz.



1/10/11 Release Notes for version 1.11.11.0110 maintenance release

- New Features
-  End Device Configurator: Support for new expanded HHF1000 firmware version.

- Bug Fixes
-  End Device Configurator: Changed wording of wizard screens to make sense with HHF1000.
-  End Device Configurator: Fixed bug that inserted an extra space into HHF1000 settings write.
-  End Device Configurator: Added delays between commands when writing HHF1000 settings to prevent collisions.
-  End Device Configurator: Reworked serial communication for HHF1000 for better reliability.


1/14/11 Release Notes for version 1.11.11.0114 maintenance release

- Bug Fixes
-  End Device Configurator: Changed "Connector Address" to "Transmitter Address"
-  End Device Configurator: Disable Back button during Step 4 and Step 5.  It's not possible
	to go back at this point, and pressing back previously caused the program to become stuck at
	that step.
-  End Device Configurator: HHF1000 - Changed interval to be an up/down box, allowing 1-60 seconds.
-  End Device Configurator: Cancel button is now called Exit.

1/20/11 Release Notes for version 1.11.11.0120 maintenance release

- Bug Fixes
-  End Device Configurator: HHF1000 - Fixed bug that caused wireless transmit interval to not be programmed.
-  End Device Configurator: HHF1000 - Changed message text on final screen.
-  End Device Configurator: HHF1000 - Increased reliability of writing commands to HHF1000.
-  End Device Configurator: Added workaround for .NET issue that causes uncatchable exception when USB cable is unplugged before exiting program.

1/24/11 Release Notes for version 1.11.11.0124 maintenance release

-  Added Km/h, m/s, MPH units for HHF1000.
-  Added workaround for "USB cable unplugged" .NET crash for TC Central.

3/8/11 Release Notes for version 1.11.11.0308 maintenance release

-  Corrected bug causing part of the cursor to stay visible on the chart even after it was disabled.
-  Corrected bug causing mouse wheel zoom of the chart to stay enabled even after it was disabled.

6/20/11 Release Notes for version 1.11.11.0620 release
(test release only)
- Test version with 64-bit compatibility.
- Included latest USB drivers.

7/21/11 Release notes for version 1.11.11.0721 release

- Compatibility with 64-bit Windows 7
- Added "Check For Updates" to the Help menu. When a new version is available, the user will be directed to the TC Central folder on the Omega FTP.
- Included latest USB drivers.
- Clarified configuration of receivers that have analog output: "Address" is now labeled "Transmitter Address".
- Fixed crash when closing application when a USB device was never plugged in.

9/1/11 Release notes for version 1.11.11.901 bugfix release
- Fixed bug which caused Display Units to revert back to default after a transmitter was turned off.
- Fixed bug causing tab delimiter option to not work.
- Fixed missing Logging Units labels, making it more obvious that they can be changed and are separate from Display Units.
- Fixed crash when starting a data log session using channels that don't currently have a device transmitting.

9/23/11 Release notes for version 1.11.11.923 bugfix release
- Expanded allowable UWPC scaling values to -50,000 to 5,000,000.
This allows the software to support, for example, a device whose analog output starts at 1V instead of 0V.
- Transfer functions no longer update with every key press, this was causing some display issues.
Transfer functions update when switching to another text box, or by pressing the new Calculate button.

10/28/11 Release notes for version 1.11.11.1028
- Added support for MWTCD. The End Device Configuration Wizard can be used to setup and download data logging files.
- For UWTC-REC4 firmware 110607 and higher, added ability to set analog output to Ambient temperature.
- Compatibility with UWTC-REC4 firmware 110607 and UWTC-REC6 firmware 110607. When used with those receiver versions: Decimal places can 
now be used when setting the alarm setpoint and deadband, and UWPH alarms no longer need to be manually scaled by 100.
- Added "Copy Graph To Clipboard" to graph context (right-click) menu.
- Added ability to change Chart Title.
- Fixed crash when reading setting from a UWTC-REC2 or UWTC-REC4 whose analog output units are set to %RH.
- Splash screen now shows full version number.

12/09/11 Release notes for version 1.11.11.1209
- Thermocouple transmitters now show up as "UWTC/MWTC" in the "On the Air" window, instead of "UWTC".
- Added support for MWTCD-868S to End Device Configuration Wizard.

3/30/2012 - Release notes for version 1.11.12.0330
- Fixed compatibility issue with Windows XP 64-bit.
- Fixed crash some customers experienced when choosing "Configure" on a channel box while the device was not transmitting.
- Corrected frequencies displayed for MWTC-REC6-915 receiver.

9/12/2012 - Release notes for version 1.11.12.0912
- Fixed error where Universal Wireless End Device Configuration Wizard (UWTC) would misidentify UWTC-REC1+ as unknown endpoint device if first device in serial port probes

1/8/2013 - Release Notes for Version 1.11.13.0108
- Fixed error where Universal Wireless End Device Configuration Wizard (UWTC) would write small negative values stored in MWTC log as large positive values in log file.

2/5/2013 - Release Notes for Version 1.11.13.0205
- Added additional response to identify new XBEE-PRO-XSC (S3B) radio which is replacing end of life 900 MHz radio.